This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4130: Require ultra low noisy single to differential amplifier

Part Number: THS4130
Other Parts Discussed in Thread: OPA820

Hi Team,

I require low noisy(<1.5 nV/root Hz) single to differential amplifier like THS4130 which should have higher slew rate & BW at least 500 MHz.

My application is:

input signal range 0.5 MHz to 25 MHz

input voltage: 500uV to 2 Vpp

Amplifier should support unity gain & max gain up to 10 V/V

Should also support 1 M ohm input impedance at least.