Part Number: OPA187
Hi,
On the OPA187's datasheet revision of July 2017 it says in the absolute maximum rating section, that the differential input voltage should not exceed plus or minus 0.5V. if I understand correctly the reason for that is a pair of diodes connected between the two input pins.
On the revision currently available on the website is says no such thing, although that pair of diodes still appears to exist.
Can you explain why the latest version of the datasheet does not say anything about the differential input voltage?
Thanks,
Shaked