This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO224: About ISO224 output noise peak

Part Number: ISO224


HI team,

My customer has problems in circuit design.

When he use iso224, Its output has some short-circuit noise peak, the highest one is -87db. In particular, when he change another Iso224b,the noise peak will appear at different frequencies. For example, the noise peak of this chip at 430hz, and the noise peak of another chip at 1kHz.

His circuit is as follows,Thank you.