This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA253: Could INA253 be a low-side current measurement design?

Part Number: INA253

Hi Sir,

As the title, quick question. Could INA253 be a low-side current measurement design?

Please refer to the simple diagram.

Thanks,

George

  • Hello George,

    As specified on the INA253 datasheet, the common-mode input voltage range of the INA253 is from -4V to +80V. Therefore it can be used in either high-side or low-side applications.

    Best regards,

    Ian Williams
    Applications Manager
    Current Sensing