Part Number: LM231
Other Parts Discussed in Thread: LM331
Hi,
my customer is using AD7740 for voltage to frequency converter.
I wonder if LM231 is the best to promote against AD7740? It seems that our temperature range is narrower.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Howard,
The LM231/LM331 is the only TI V-to-F converter that is designed to operate directly from a low voltage, 5 V supply (4 V minimum). Therefore, it the one option for low voltage applications that the AD7440 might be used in.
The AD7440 K grade temperature range, according to the datasheet is guaranteed from 0°C to 85°C. It is –40°C to +105°C for the automotive grade device. The LM231 datasheet Operating Ambient temperature is specified as −25 Min, +85 °C Max, in the Recommended Operating Temperature Table 7.3. The AD7440 electrical tables specify the parameters with TMIN to TMAX. While the LM231 Electrical Characteristics table specifies TA = 25°C, unless otherwise specified. Many of the LM231 specifications are specified for TMIN ≤ TA ≤ TMAX.
The choice that the customer makes comes down to which electrical parameters are most important over temperature in the application, and of course cost.
Regards, Thomas
Precision Amplifiers Applications Engineering