Other Parts Discussed in Thread: XTR115
I am designing a sensor with a 4-20mA output and I plan to use the XTR115. I know the the XTR115 has an internal 5V regulator, but my sensor circuitry requires at least 7V. If I connect a load between the V+ pin and IRET pins, will the XTR115 still operate correctly? If so, I can connect the VIN pin of an external 7V regulator to V+ and the GND pin of the regulator to IRET and create the 7V that I need.
Regards,
Leonard