Part Number: INA282
Hi! I want to measure alternating currents from 5mA to 1A from 220VAC and thought of INA282. I want to use it on low side as in the schematic below, is it possible?
The circuit will be "open" until the triac receives signal, then it "closes" for a 300ms time, then "opens" again. It is a circuit to test a differential circuit breaker.
I will use a microcontroller powered by trasnformer and 5V regulator.
Regards,
Martin