Other Parts Discussed in Thread: INA139
Hi,
Good day. I hope everything is fine.
Our customer wants to use the INA169 (INA169NA/250) and they noticed that the information about the operating condition is not consistent. On the packaging information (page 21) of the datasheet, it shows that the operating temp is –40°C to +125°C. However, on other parts of the datasheet it says the op temp is just –40°C to +85°C (page 1, page 6..). In line with this, we would like to know which is the correct operating temperature of INA169.
Furthermore, on section 6.5 Electrical Characteristics, there is a parameter "Operating" (temperature), which is in the range of –55°C to 125 °C. I would like to know which this parameter refers to. I would appreciate if you could help us on this inquiry.
Thank you and stay safe.
Regards,
Cedrick