This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO124: Difference between ISO122 ans ISO124

Part Number: ISO124
Other Parts Discussed in Thread: ISO122, ISO224

Hello team,

ISO124 seems to have been released after ISO122.

What are the improved characteristics of ISO124 from ISO122?
It only looks like the difference in gain non-linearity (ISO122 max 0.02% vs ISO124 max 0.01%), is there anything else?


Which product is recommended for the new design?

Regards,

H.Someno