This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA381-Q1: Input current at RESET

Part Number: INA381-Q1


I have a question related to the input impedance in the following E2E post.

https://e2e.ti.com/support/amplifiers/f/14/p/917744/3391574#3391574

In electrical characteristic table on INA381-Q1 datasheet, there is the specifications of following parameter.

This parameter seems to be explaining the input current flowing into RESET pin. 

If so, input impedance range of REST pin is several Mohms range, not 100Mohms range.

How do you think about it?

Regards,

H.Someno

is this parameter