This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

150V differential DC signal acquisition solution

Other Parts Discussed in Thread: INA149

Demand: DC signal, accuracy 0.1%.
Help recommend a plan.
The existing scheme is to use a resistor divider network plus a differential amplifier. The input impedance of the differential amplifier is generally within 1MΩ. The sum of the resistors of the voltage divider network must be less than 1kΩ. The resistance power is 22W, which is too large. The resistance is not good for selection.