Part Number: TLC271B
Hi Experts,
My customer is asking about VOH accuracy on each device. VOH is defined as below and the actual VOH varies, I think.
A device's VOH is 3.4V and other device's VOH is 3.6V etc. What is the VOH accuracy for each device? For example, 3.4V +- 10% or 3.6V +- 10%. The condition is fixed VDD(5V) and whole temperature range.
This opamp is used to detect photo sensor(I-V). When photo sensor is on, TL271B outputs at its the maximum VOH and it will be converted by ADC. They need to calculate the output accuracy to get industrial certification.
Regards,
Uchikoshi