Part Number: LM2901
Other Parts Discussed in Thread: LM393, TLV1704
Hello,
I am a development electronics engineer in a company in Nuremberg, Germany.
We are at a development stage when we cannot change the circuit without extensive tests anymore.
We have an issue regarding the common mode input range of LM2901. We are exceeding the prescribed range of 0 to Vcc-2V at inputs.
In our circuit the supply of the comparator is connected to 3.3V.
Please consider this scenario:
Comparator minus input is in common mode range.
Plus input connected to a square wave (Ton~=Toff) between 162mV and 2.6V and a period of 100µs, so we exceed the common mode by 1.3V.
It is most important for us that the output toggles between low and high states with every input period, not necessarily looking square shaped.
Will the ouptput toggle in the temperature range -40°C to 105°C? How much delay will we have at the edges?
As in our case one input exceeds the common mode range as much as 1.3V, how much will the deviation from the datasheet be? (values from datasheet: Input bias current (Iib): Max -500nA, Input Offset Voltage (Vio): Max 15mV, Response time: 1,3µs)
Thanks much and yours sincerely