This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternative of OPA621

Other Parts Discussed in Thread: OPA820, OPA620

Hi Team,
My customer is looking for a product with the similar or better performance than the already discontinued OPA621.
Please propose an alternative part.
Key parameters that they need are Input noise, High BW, +/-5V operation in small package.
The following shows the key specifications for OPA621.

- Noise
  Voltage: 2.3nV/√Hz(fo = 1MHz to 100MHz)
  Current: 2.3pA/√Hz(fo = 10kHz to 100MHz)
- Gain-Bandwidth Product: 500MHz
- Offset voltage ; +/- 100uV
- +/-5V operation
- Stable in Gains : >=2V/V
- SOIC 8pin

Regards,
H.Somneo