This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

part number

Other Parts Discussed in Thread: OPA2333, XTR117

Hello,

I send this email to ask part numbers of specific chips I have.

Codes are written on ICs, but I could not find out the certain part numbers.

I thought these codes are not the part numbers but serial numbers or others.

One is 'I333A TI 61K A4DE' (or '1333A TI 61 A4DE)

and the other is 'BQZ TI K 713K' (or 'BOZ TI K 713K').

These codes are not sure because these chips are too small to clear the characters.

(e.g. The above 'B' might be 'R' or '8')

Additionally, both ICs have 8 pins.

I would appreciate it if you let me know the exact part numbers of these ICs and the spec sheets.

Thank you,

Namho Kim