Hi, I'm having trouble with IIB simulations for OPA2376. Configured as a unity gain buffer, I see -5 to +5 nA of input bias current when sweeping VIN from 0 to 5 V (using DC Transfer Characteristics) when modifying the reference design here: www.ti.com/.../sboc261. It should be much lower according to the datasheet. When I use the model
, I see IIB of < +/- 20 pA as expected.
Why are the models different? Is one incorrect?