Part Number: OPA2187
Hi Team,
My customer now use OPA2187 and meet the zero -drift problem. They test the zero- drift is 7mV 25 ℃, higher than datasheet's value 10µV, 0.001µV/C˚
Could you please give some advice? thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2187
Hi Team,
My customer now use OPA2187 and meet the zero -drift problem. They test the zero- drift is 7mV 25 ℃, higher than datasheet's value 10µV, 0.001µV/C˚
Could you please give some advice? thanks!
Hi Amelie,
Michael's response is to the point; we must see the OPA2187 circuit schematic to be able to provide assistance. Along with the schematic please be sure to include power supply levels applied to the V+ and V- pins, any applied input voltage level, and any output load conditions during the offset/temperature test.
One quick check the customer can make is to connect a 10x probe/DSO to the OPA2187 output and check for high frequency oscillation. If the circuit is unstable and oscillating that will corrupt the offset measurement. If that proves to be the case, then there is a circuit design problem.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Amelie,
We haven't heard from you in a while. We hope the issue was resolved. I am going to close thing thread now, please reply to reopen if you have any additional questions / information.