Part Number: INA333
Hello,
According to the datasheet 8.2.2.5 Input Bias Current Return Path, it describes that: With higher source impedance, using two equal resistors provides a balanced input with possible advantages of lower input offset voltage as a result of bias current and better high-frequency common-mode rejection, so I made a circuit which the signal source impedance is 100Kohm, but the output is not correct, if I changed the internal resistance to 0ohm or connect the resistor to one input like thermalcouple application, the output is right. But it is used to the differential source impedance is low. Please help to analysis.
Best regards
Kailyn