Other Parts Discussed in Thread: TLV3011
Hi,
We are using TLV3011-EP comparator with internal reference to detect undervoltage on a supply rail and the compartor is powered up with 5V.
It is observed that the output got latched from LOW to HIGH when the temperature was decreased from 25degC to -55degC and there was no change in input voltage or the supply to the IC.
Can you please let us know if there is any issues with TLV3011 internal reference voltage with respect to temperature?
Thanks,
Midhun