Hi,
My application measurement range is from 10mA to 5A with a 10mohm sense resistor. Vcm = 12V.
I'm using GND as the INA reference for unidirectional sensing.
The ADC Vref = 1.8V.
The INA190A1 specifies a 3mV (max) at zero input current, which translates to a 12mA error at zero input current given 25V/V gain and 10mohm shunt.
Should I treat this 3mV negative rail headroom as an offset error or a noise floor? If my sense current is 12mA, will the INA Vout be 6mV (worst case) or 3mV?
Would you recommend using GND as a reference or should I offset the output with a 100mV Vref instead to avoid the negative rail. This INA 100mV Vref will be generated with the 1.8V ADC reference for ratiometric measurement. Please advise.
-Kelvin