Other Parts Discussed in Thread: ADS1232, OPA277, INA333, INA828, INA317
Hi, I'm an electronics novice, I wanted to work on a load cell and I'm considering which amp is best suited.
Load cell 1Kg (max), 1mV / V, ADS1232 to read the values, working voltage 3.7V (lithium battery).
I wanted to use the one in the OPA277 datasheet as an amplification circuit, to be connected to my ADS1232, but recently I saw that the INAXXX amplifiers are much more practical and complete, all in a single package, so I would like some advice: it's better to use 2 OPAs or an INA for a load cell? And which INA is more suitable for a load cell? I was currently reading the documentation on the INA333, could that be fine?
Thank you