Other Parts Discussed in Thread: OPA2189, OPA1632, , THS4541
Hello,
I am trying to make some noise simulations in TINA-TI of my designed instrumentation amplifier circuit made with the OPA2189 and the OPA1632.
According to the book: Operational amplifier noise by Art Kay, inverting and non-inverting amplifiers have the same noise gain of 1 + (Rf/Ri), while the signal gain is different.
An inverting amplfier with a signal gain of 1 has a noise gain of 2.
When i calculate the noise of only the OPA1632 fully differential amplifier, the noise reffered to the output (RTO) is twice the noise refferend to the input (RTI). The noise simulation in TINA-TI gives the correct output noise and total noise indicating the correct use of the noise gain but the input noise is not 2 times smaller than the output noise, it is the same value assuming the use of the noise gain of 1.
When the OPA2189 and OPA1632 as instrumentation amplifier is simulated i expect that the output noise of the first stage (OPA2189 with signalgain = 100 and noise gain = 100) is multiplied with the noise gain (=2) of the second stage (OPA1632 with signalgain = 1 and noise gain = 2), but the simulation gives the same noise at the output of stage 1 and stage 2.
So the OPA1632 noise simulations used the noise gain of 2 to get the correct output and total noise, but the input noise en the output noise of the previous stage is not correctly using the noise gain of stage 2 the get the correct output noise of the compleet circuit.
Also a test with the OPA2189 as inverting amplifier (signal gain = 1 and noise gain = 2) gives the correct output and total noise, but the incorrect input noise.
Am i doing something wrong with the noise simulations or is TINA-TI not correctly using the noise gain?
Kind regards,
Wesley Pot