This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the diffierence between -DGKT or -DGKR. And what is G4 at the end?
Thank you for taking time.
Steven
Hi Steven,
The OPA381DGKT signifies the MSOP-8 package supplied on a small, 250 device, tape and reel. The OPA381DGKR is the same device supplied on a large, 2500 device, tape and reel.
The G4 designation came about during the period when manufacturing was transitioning to green, lead-free packaging. The G4 was used to distinguish this material from traditional packaged devices that did not use green, lead-free packaging. Now that the OPA381 is only available green, lead-free it is really a holdover from the transition period. But because customers have their BOMs set up for one, or the other, part number both part numbers are maintained.
Regards, Thomas
PA-Linear Applications Engineering