This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3330-Q1: Possible Typical Application Datasheet Error

Part Number: AMC3330-Q1

Hello,

I was reading the datasheet for the AMC3330-Q1 and I noticced what may be an error in the Application Section. In table 2, The RL11 annd RL12 values for a 120V AC Line is written as 845 MΩ, whereas the value for a 230V AC line is 1.62 MΩ. Is the value for the 120V supposed to be 845 KΩ, not MΩ?

Thanks,

Kyle