Hi!
I have some questions regarding the THS4524 opamp.
I plan to use a single +5VDC supply for the opamp. The input signals are differential (symmetrical) signals with a common-mode voltage of 0V. This violates the absolute maximum ratings in the THS4521 datasheet, but is this still ok? I've seen this configuration with single-ended inputs, but not with differential inputs.
The opamp is going to drive a PCM4204 ADC, which needs a common-mode level of 2.5VDC. The THS4521 datasheet states that if Vocm is left unconnected, the common-mode voltage will be set to midsupply (2.5V). Is this good enough, or do you recommend to use the Vcom output from the ADC and connect it to the Vocm of the opamp?
thanks