This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC27L9CDR: Noise side effect in steady state and transcient state

Hi sir, 

Could you pls kindly reply below question from my customer? Thanks a lot!

1. When Vdd=16V in Steady state, is there any issue or side effect if noise overpass a little based on spec?

2. When Vdd>16V, <18V in Transient state,<18V, is there any issue or side effect if noise overpass a little based on spec?

BR, 

Sean Liao

  • Former Member
    0 Former Member

    Hello Sean,

    Thank you for your question.  Can you please clarify what is meant by "if noise overpass a little based on spec?"

    Which specification are you worried about?  Do you mean the noise is going beyond the V+ supply rail?  If you have a schematic or input signal waveform, that would help.

    Regards,

    Daniel

  • Hi Sean,

    Looks like this is being handled via email. Closing this thread now.