This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA233 calibration issue with EVM board GUI

Part Number: INA233

Hello,

I am having trouble in INA233 current calibration with the EVM board/GUI and below is my detail steps:

1.Use the equation in data sheet to calculate the Current_LSB=(Maximum Expected Current)/2^15=15A/2^15=457.7uA/bit,then I choose 1mA/bit as the
Current_LSB.
2.Use the equation in data sheet to calculate the MFR_CALIBRATION value=0.00512/(Current_LSB*Rshunt)=0.00512/(1mA/bit*0.5mΩ)=10240
(Decimal)/2800(Hex)
3.Power up the INA233 EVM board,start the GUI and write 2800(Hex) into the MFR_CALIBRATION successfully.
4.Connect a 0.5 mΩ external resistor to the IN+/IN- terminal on INA233 EVM board and apply 2A current accross the resistor.

5.Read the VSHUNT_OUT value on EVM GUI and the vlaue is 0.0275V which is correct.

6.Read the READ_INN value and the vlaue is 7FFF/32767 which I suppose is abnormal.

Below is my questions:

Since I can read the VSHUNT_OUT value on GUI directly,is there somewhere on GUI I can read the current value directly as well?If not,where can I read the current value on GUI and how to translate it into a decimal value in ampere?