Part Number: INA226
Other Parts Discussed in Thread: TVS1400
Hi, staff
The device was damaged as a result of the test that applied ESD of IEC61000-4-2 to IN+ (VBUS) and IN- terminals of INA226.
We plan to use TVS for ESD protection.
I think that connecting the TVS (ESD protection device) near the INA226 pin rather than near the INA226 pin is more effective in eliminating ESD.
Is there any problem with my opinion?
Also, is there any TVS that can be introduced at TI?
Vrwm is 12V.
best regrads
cafain