Part Number: PGA309
Other Parts Discussed in Thread: XTR115, , PGA308
Hello
Application Report:SBOA107B proposes a 4-20mA loop system.
This is a combination of sensor, PGA309, EEPROM, XTR115.
However, PGA309 and XTR115 use about 1.9mA current.
Operating current that can be used by the sensor and EEPROM is 2.1mA or less.
Previously proposed EEPROM was 24LC01B
It uses max 1mA current
Therefore, Operating current that can be used for the sensor is small at 0.9 mA or less.
I want to reduce the operating current of the EEPROM so that the sensor can use more current.
If you have,Please tell me the EEPROM that can be combined with PGA309 without any problem.
Best regards,