Part Number: INA821
Other Parts Discussed in Thread: ISO124, OPA2141, , INA188
Hi,
I have a DC voltage of +-120mV to monitore. I am searching for some INA with very low 1/f noise (we measure DC), a very low initial offset, but we can remove some offset by (software) calibration. The full scale output voltage should be +-12V, fed into a ISO224B. The source impedance is < 2k. Supply voltage is +-14V, very clean, made locally by low noise LDOs.
The input signal is switched on/off and changes polarity, so the amp should have sufficient step resonse, the ADC sampling rate is 15ksp.
A simulation gives 1.6µV output noise for 100 Milliherz, but how much rms noise will I see in a bandwith of 7.5kHz starting at DC?
The signal ends up in a 24Bit ADC with 15ksp.
Thanks for helping.
Current solution: A OPA2141 pick up the signal, g=100, passes it to 2 x ISO124 (which formed an isolated full diff amp). With this circuit we get -95dB SN when we analyze the output of the ADC.
The new circuit should be simpler, cheaper and should have a better SN (we hope).
With best regards
Gerhard