Part Number: INA212
Hi,
We have designed in the INA212 into our system, and are noticing the devices are drawing power when we have V+ grounded.
Essentially we are powering the device V+ through a 3.3V GPIO, so are able to ground V+ when needed. REF always has 1.5VDC applied to it. IN+ and IN- always have 0V/3.3V toggling. Do we expect the INA212 to consume power when V+ is grounded, and there is a voltage on VREF?
I have physically removed the 2 INA212 devices from our boards, and can observe a drop in power of ~16mW when they are removed. Without knowledge of the internal workings of the devices, are the devices expected to draw power with V+ set to 0V, and REF set to 1.5VDC? Any help you can offer would be greatly appreciated.
Thanks,
Andrew