This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6704: 3.3V R2R op amp with integrated resistors for difference amplifier like LMH6704

Part Number: LMH6704
Other Parts Discussed in Thread: OPA2832, INA597

Hello,

I am  looking to make a simple subtractor for signals below 1 MHz for four channels. is there a chip that can do that that is more compact than a regular quad op amp with 8 resistors where all the resistors are integrated on chip? I inserted a picture from the LMH6704 which is the general idea. I would need 3.3V Rail-to-rail.

Is there an easy way to filter my requirements in the parametric search at www.ti.com/.../products.html

Frank