Dear team,
I cannot find *TAPE AND REEL INFORMATION* of LM2903PSR in datasheet.
Could you share with me?
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sorry Ben
I see that it is missing in the datasheet as well for the LM2903PSR in SO package.
we will work with our manufacturing team to get a response for you.
Chuck
Hello Ben,
There seems to be an issue with this package, as it has also dropped off of many other datasheets.
Here are the tables as they should have appeared:
TAPE AND REEL INFO
Device | Package Type |
Package Drawing |
Pins | SPQ | Reel Diameter (mm) | Reel Width W1 (mm) |
A0 (mm) | B0 (mm) | K0 (mm) | P1 (mm) | W (mm) | Pin1 Quadrant |
LM393PSR | SOP | PS | 8 | 2000 | 330 | 16.4 | 8.35 | 6.6 | 2.4 | 12 | 16 | Q1 |
LM2903PSR | SOP | PS | 8 | 2000 | 330 | 16.4 | 8.35 | 6.6 | 2.4 | 12 | 16 | Q1 |
LM2903PSRG4 | SOP | PS | 8 | 2000 | 330 | 16.4 | 8.35 | 6.6 | 2.4 | 12 | 16 | Q1 |
LM393APSR | SOP | PS | 8 | 2000 | 330 | 16.4 | 8.35 | 6.6 | 2.4 | 12 | 16 | Q1 |
LM393PSRG4 | SOP | PS | 8 | 2000 | 330 | 16.4 | 8.35 | 6.6 | 2.4 | 12 | 16 | Q1 |
TAPE AND REEL BOX DIMENSIONS
Device | Package Type |
Package Drawing | Pins | SPQ | Length (mm) | Width (mm) | Height (mm) |
LM393PSR | SOP | PS | 8 | 2000 | 367 | 367 | 38 |
LM2903PSR | SOP | PS | 8 | 2000 | 367 | 367 | 38 |
LM2903PSRG4 | SOP | PS | 8 | 2000 | 367 | 367 | 38 |
LM393APSR | SOP | PS | 8 | 2000 | 367 | 367 | 38 |
LM393PSRG4 | SOP | PS | 8 | 2000 | 367 | 367 | 38 |
We are investigating.
Hi Paul,
The Tape size customer received is 16*12mm not 16*8mm you shared with me in last mail.
Could you double confirm with this?
Ben