This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS6222: If I use two of these devices, can I connect the inputs in parallel?

Part Number: THS6222


If I connect the pin 1 from the first chip to pin 1 on the second, and do the same with the pin 2s, will this cause any issues?

Thanks,

Lauren