Part Number: LMV601
Hello,
We use the LMV601 as an amplifier for signal coming from a pH probe.
When soldered by hand on our prototypes, it works great. However when it comes out from our desktop reflow oven, the impedance is too low to handle correctly the voltage generated by the pH probe which has an output impedance of about 250 MOhm.
It looks like after reflow, the 20 fA of input bias current stated on the datasheet is not relevant anymore.
Other parts works perfectly and the temperature of the oven is good. The peak temperature is 245 deg. C for only 15 seconds. The reflow profile is compatible with Level-1-260C-UNLIM.
We can't test the input current as we don't have the right equipment for such low values.
Is it a known issue ? Is there a solution other than soldering this part by hand ?
Thanks !