Part Number: TLV8801
Hi
I have see one problem , first please check schematic is right?
The problem I have encountered is that the output voltage will rise 0.5~0.6V,
Please have suggest ? power ripple about 80mV..
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey JC,
Can you clarify what the voltage is at PP3300? I assume it is 3.3V.
Additionally, what is the signal coming from the USB_C0_CC1? Can I assume a 1V sine wave?
All the best,
Carolina