Part Number: ISO124
Other Parts Discussed in Thread: ATL431LI, , ISO224
I wanted to use ISO 124 to obtain an isolated analog output for an analog input. I have a doubt that can the supply be 18V/12V and 0V at Vs1+,Vs2+ and Vs1-,Vs2- respectively or is it required to supply +18V/+12V and -18V/-12V respectively. In the datasheet it is mentioned that the absolute max rating of Vin pin is 100V so can I give an input of 0-18V or 0-12V in the input or as mentioned in the description I have to give a 0-10V input.