This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA300EVM: Test Report for HYS=2mV, 4mV, 8mV

Part Number: INA300EVM

Hi Team,

My customer is looking forward a test report on EVM with setting HYS=2mV, 4mV, 8mV..

This is used to add this device in AVL. Kindly help to provide this. 

If not, do you have a clear test procedure and what result you are looking forward for refrence?

Thanks for your help . 

  • Hello Beginner,

    Thanks for reaching out on the forum.  We do have a user guide that tells you how to use the EVM here.  As for an example of what the hysteresis does, it re-asserts the alert to low when the device is in transparent mode and the output voltage has dipped below rlimit*ilimit-Hys.  So if rlimit*ilimit = 2.5V, and hys pin is set for 4mV, then after the initial trigger, the alert will remain high until Vout ≤ 2.5V-4mV=2.496mV.