Part Number: INA190
Hi
I am using the INA190 to drive the input of a sigma delta ADC with built in MUX. This means that the ADCs MUX switches to the built in capacitor (of 25pF) and the INA190 has to provide the current. I am optimizing the time for the INA190 to settle and with SPICE simulations and verifications on hardware have seen that loading the output of the INA190 with a resistor improves the settling time. Now I have two questions:
1) Can you confirm that this is a good method for decreasing the settling time when the INA190 has to drive a capacitive load of 25pF which is attached and detached by a MUX? Are there other recommended ways?
2) What is the maximum resistive load the INA190 can drive? The datasheet only mentions a R_L of 10kOhm as test conditions.
Thanks
Dominic