Other Parts Discussed in Thread: LM393
Hello,
We are planning to use OPA2237 as a comparator where the input signal is not slow moving, but changes abruptly at the non-inverting input to a negative value. I am posting this question in the Amplifier forum as I was advised to do so by the Comparator engineers. The package we are using is 8-pin SOIC where only one opamp is being used.
OPA2237 is intended to replace LM393 in our circuit that is already in production. The LM393 was getting damaged, due to the negative input voltage that it saw at its non-inverting input.
We decided to use OPA2237 as we needed a device whose abs. max input voltage rating was around -0.8V (where OPA2237 guarantees -0.7V). Also, we needed a power supply value > = 28V. OPA2237 was the only one to satisfy the requirement.
Attached is the application circuit. We wanted to make sure it won't get damaged due to the negative input voltage. Is there a clamping diode inside it that will clamp the non-inverting input to a safe level?
We also wanted to make sure that opamp won't oscillate when used as a comparator. If there are any suggestions you have, they would be greatly appreciated.
Also, if there is anything else we need to be careful of, when using it as a comparator, please advise. Would greatly appreciate your response.
Kind regards,
Nitish AgrawalOPA2237_as_comparator_TIE2E.pdf