This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA858DSGEVM: OPA858DSGEVM

Part Number: OPA858DSGEVM


Bonjour, j'utilise la carte d’évaluation OPA858DSGEVM pour amplifier mon signal qui est issu d'une autre carte evaluation d'un capteur SiPM, malheureusement je trouve un gain de 1 au lieu d'un gain de 7 dans la configuration non inverseur. je vais expliquer comment je câble la carte d’évaluation ( pour les alimentations j'utilise VCC= 2,5v et VEE= -2,5v) , mon entrée cable sma qui sort du capteur et il rentre sur le pin J2 (IN+) pour le pin IN- je mets rien car dans la datasheet il est connecté a la masse via R3. merci pour votre aide svp?  

  • Traduit par google:

    Hello,

    I am using the OPA858DSGEVM evaluation board to amplify my signal which comes from another evaluation board of a SiPM sensor, unfortunately I find a gain of 1 instead of a gain of 7 in the non-inverting configuration . I will explain how I wire the evaluation board (for the power supplies I use VCC = 2.5v and VEE = -2.5v), my sma cable input which comes out of the sensor and it goes into pin J2 (IN +) for the IN pin - I put nothing because in the datasheet it is connected to ground via R3. thank you for your help please?

  • Thanks for the translation Kai!

    El Bouanani,

    Can you share what sensor you are using here? Specifically what is the output impedance of the sensor?

    Also are you accounting for the loss in gain from the output voltage division? (Assuming you are using a 50-ohm measurement device).

    Best,

    Hasan Babiker