This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA233 read current instable issue

Part Number: INA233


Hello,

i use INA233 device, before calibration current, observed INA233 read current drift between 1995mA ~ 2005mA (Actual load current is 2000mA).

do you what is problem is? thanks.INA233 Issue .ppt

  • Hello Jimmy,

    The reason for this behavior is simply due to Gaussian noise with the load current. Increasing the number of averages will begin to digitally filter out noise in the load current. This is similar to increasing conversion time as seen in Figure 24 of datasheet.

    The amount of noise in the INA233 measurement will get worse if you have chosen a very small current LSB value as well.

    If you think the noise is outside of spec and need an analysis, then you need to consider how to determine the true noise of the load current using some much less noisey instrumentation or devices and consider the thermal noise of the shunt.

    Adding an input filter with a capacitor as close as possible at the input pins of INA233 will also aid in low-pass filtering high frequency noise.

    Hope this helps.