Hello,
I am trying to diagnose a DC component problem. I am performing RF immunity tests with TLV2422, and the test fails because there is a DC shift in the output. The amplifier is configured in a voltage follower/buffer circuit. The DC shift @ RF frequencies is greater than 20mV in most cases. This is undesirable because the signal that I am buffering is smaller than the DC offset.
Further experimentation shows that the TLV2442 does not produce the DC shift during RF immunity tests. The amplifiers are pinout compatible so the same layout and circuit board were used to perform the experiment.
Can someone comment on the difference between these two amps? The datasheets and equivalent schematics look nearly identical, except the 2442 is a faster amp and uses more power.
Thanks,
Keith