This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM393: LM393 comparator usage in the resistance meter range control

Part Number: LM393


LM393 is to me familiar from 1970 -1985 when I was a designing Nokia Capacitor Factory devices. 

It was then only DIP8 device, now I use SO8 devices, but the operation is same.

This design needs  a positive feedback, so that I got very sharp range change.

Without positive feedback LM393 was not working properly just when the both inputs ( + and -) were almost similar.

The meter needs automatic star and  automatic range control, but it used very old AD-device ICL7106, which needed two power supply voltages,

but I have only one 3 V battery .

It need to use very little current 300uA when the device was in not working.

It used about 10mA when everything was working.

I have designed these kinds of the devices already many years, but now I have no oscilloscope available.

It was broken,

Here are my memories ( add : )

http  //remotesmart.wikidot.com/hewlett-packard

Regards

Pekka Ritamaki

.