Other Parts Discussed in Thread: LMP7300, TL7712A, TLV6710
Hi team,
My customer is looking for a comparator. Does TI have a comparator with the same function as TLV6713, but it is inverting?
He created a Sealed Lead Acid Battery Deep Discharge Battery Protection circuit.
If the SLA Voltage is above say 10.5V, the RELAY is closed and SLA Battery Voltage is passed to the circuit.
And if the SLA Voltage is below say 10.5V (with a bit of hysterysis), the RELAY is open and the SLA Battery Voltage becomes disconnected - except for current to power the Deep Discharge Protection circuit (say 50uA).
The TLV6713 Comparator would be perfect - if only it was inverting.
36V plenty for a 12V (15V max) SLA Battery.
Open drain handles 25V
Open drain sinks 40mA (Relay)
Internal reference
Very low power
He couldn't see anything useful under the Battery Protection section.
so he want to find a comparator that would work for this application. Please advise.Thank you.