Other Parts Discussed in Thread: XTR110
I am making a 0-5V to 4-20 mA converter.
I bought this IC and just for trial made the same circuit givein under Applications in the datasheet (0-10V to 4-20mA).
However the circuit gives varying current for for varying Vcc but doesn't change with change in Vin as it should.
I also tried the 1-5V and 0-5V to 4-20mA circuits but same result?.
Also pins 15(Force) gives o/p of 13.3V , pin 12(Sense) give around 9.5V while pin 3 has voltage of 3.75V for Vcc of 14V.
Please guide me.