Dear TI expert,
My question is how to improve the accuracy of Peak Detector as high as posssible?
My application is as the schematic below.
I want to sense the peak of v=v(t). As can be seen, v rises form 0 to peak within around 200ns. The peak is within the range of 650V and 1050V. It is first scaled down with ratio 1/350 by RC divider and then sensed by the amp based peak detector. R is for the stability of OP1. Since v is periodic and it happens every 200us and its peak should be sensed every period, SW1 is employed to discharge C and make the peak detector work every cycle. OP2 is a follower and its output is scaled down to obtain vo2 suitable for the input of ADC.
I wonder how you suggest to improve the accuracy of the digitalized peak? From the perspectives of the configuraion of peak detector and the selections of OPs and ADC.
Best regards
Yatao