Hi,
I have used the THS4151 op-amp to create a circuit that takes two inputs and subtract them to give an output. Below is the schematic for the circuit:
R1 is where I will input a 1 MHz, 2V sinusoidal signal, and R6 is where the other input signal should come from. In this case, I grounded that input. Below is a picture of the input signal:
My problem is when I try to power the op-amp, It will oscillate, and the input signal will look like:
and the output look like this:
any suggestions?
Thank you