Part Number: LM1558
Hi Team,
I have a question on LM1558H/NOPB. Could you suggest me the component with same functionalities of LM1558H but SMT / SOIC-8 package?
Some features have higher priorities :
- double supply voltage +/- 22VDC
- low stand-by consumption (low Iq)
- slew rate 0.5V/us
- temperature -40°C/125°C
- good EMC
- short circuit protection at the output
Thank you in advance,
Riccardo