Part Number: INA226
Hi Team,
This IC has a ALERT function. It is enabled for only one feature selected in the Mask / Enable Register (06h) setting, and the ALERT limit (threshold) for that selected feature is set in the Alert Limit Register (07h).
For example, In case This IC is used in bi-directional current sensing and 80mV threshold(limit) is set for Shunt Voltage Over-Limit(SOL) , I understand hat the 80mv threshold applies to each current flowing in both directions. Is that okay?
Regards,
H.Someno